2025-03-17 7:13 PM
I’m connecting to an HT16K33 (on an Adafruit 4-digit, 7-segment display) to a NUCLEO-H755 board.
I’m connecting I2C4 SCL to PF14 (pin 19 on CN9), and I2C4 SDA to PFf15 (pin 21 on CN9).
Here's my init:
static void MX_I2C4_Init(void)
{
hi2c4.Instance = I2C4;
hi2c4.Init.Timing = 0x10707DBC;
hi2c4.Init.OwnAddress1 = 0;
hi2c4.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c4.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c4.Init.OwnAddress2 = 0;
hi2c4.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c4.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c4.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
...
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c4, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
...
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c4, 0) != HAL_OK)
...
}
I make the following call:
uint8_t buffer[] = {0x00, 0xFF, 0x3F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
HAL_I2C_Master_Transmit_IT(&hi2c4, 0x70, buffer, sizeof(buffer));
I get an error interrupt with a HAL_I2C_ERROR_AF error.
void HAL_I2C_ErrorCallback(I2C_HandleTypeDef *hi2c)
{
uint32_t lastErrorCode = HAL_I2C_GetError(hi2c);
if (lastErrorCode & HAL_I2C_ERROR_AF) {
// ACKF error
// Not acknowledge received flag
// This flag is set by hardware when a NACK is received after a byte transmission. It is cleared
// by software by setting the NACKCF bit.
__BKPT(0);
}
__BKPT(0);
},
Solved! Go to Solution.
2025-03-17 7:30 PM
Try a slave address of 0x70 << 1 (0xE0). Needs to be left-shifted.
2025-03-17 7:30 PM
Try a slave address of 0x70 << 1 (0xE0). Needs to be left-shifted.
2025-03-17 8:25 PM
Thank you!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.