2023-12-06 5:28 AM
Hello,
Actually i'm trying to mesure the pressure using LPS28DFW and arduino uno, but i have some problems, the i2c communication does not working.
Can help me please and thank you.
arduino code :
2023-12-12 11:58 PM
Hi @ljm ,
Two suggestions: the CS must be high when you are in I2C, in addition you can check if the SDO pin matches the address set.
Hope this helps
2023-12-18 6:11 AM
Hello,
I have a question.
For the LPS22DF, in fact I do shock tests, and I compare the measurement of the sensor with a reference, in a certain number of shocks I saw that the difference was 20 mbar but when I continue the test with more shocks I saw that the difference was decreased to 13 mbar, is it the membrane that has moved? or another mechanical phenomenon that has passed?
I'm applying tests of 10,000 and 20,000 shocks (between 200 and 300 g each).
Yes, I'm measuring the temperature (between 19°C and 24°C).
i'm using 10 simples,
only the sample number 8 has this deviation from 13 mbar of difference to 20 mbar and by continuing to test, it was back to 13mbar of difference.
the rest of samples are all the sample difference of measurements
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.