2023-12-07 1:03 AM
Hello,
I have applied for the ASM330LHBxx ASIL B library from ST's web, and integrated it to my program, all the functions worked fine. But the noise of GYRO has gone beyond our requirement, we used to enable the LPF in ASM330 to lower the noise.
We have checked the integration manual of AB lib, it doesn't provide a function to set and enable the LPF filter, and it forbids users to set ASM330 without using AB lib(according to the Introduction sector in the manual). Is there any method to set and enable the LPF function even though using AB lib?
Solved! Go to Solution.
2023-12-18 6:22 AM
Hi @ssdgf ,
Being a filter, LPF introduces a certain amount of delay.
The addition of this feature inside the library implies adopting a regression strategy to verify that the implemented change does not affect the unchanged, existing and previously verified parts or properties of the software library. Retesting all mechanisms is a regression strategy for example to prove that the ASIL B is fulfilled after the addition of the LPF enabling/disabling.
2023-12-12 7:43 AM
Hi @ssdgf ,
Welcome to ST Community!
In the current version of the ASIL B software library, the user cannot set and enable the LPF filter. This feature is going to be implemented in future releases of the library.
2023-12-17 7:12 PM
Hi @Federica Bossi ,
Thanks for your reply, the LPF is quite important to us now. So another question is the influence on functional safety of setting and enabling the LPF though the spi port driver directly is limited in reading and writing the LPF filter, or the other checks that safety related cannot be guaranteed to fulfil ASILB?
2023-12-18 6:22 AM
Hi @ssdgf ,
Being a filter, LPF introduces a certain amount of delay.
The addition of this feature inside the library implies adopting a regression strategy to verify that the implemented change does not affect the unchanged, existing and previously verified parts or properties of the software library. Retesting all mechanisms is a regression strategy for example to prove that the ASIL B is fulfilled after the addition of the LPF enabling/disabling.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.