2026-03-23 3:36 AM - last edited on 2026-03-23 3:49 AM by Andrew Neil
Hi, ST Community,
I am working with an LSM6DSOX on a custom board, using an ESP32S3 with the Arduino framework, and I'm unable to get the Machine Learning Core (MLC) to run.
The problem is that the output register MLC0_SRC (0x70) always reads 0x00. I am also monitoring the is_mlc_ok status bit in the EMB_FUNC_STATUS register (0x15), and it never gets set to 1. Basic communication (reading WHO_AM_I and raw accelerometer data) works perfectly.
I am not using a library and am writing directly to the registers. My initialization sequence is as follows:
Has anyone else had this problem? Is there any command or register write missing that could explain why the MLC is not starting? Or do these symptoms strongly point towards a hardware-level issue?
Thank you for your time.
2026-03-31 12:40 AM
Hi @DianaFiuza ,
Could you do a software reset and then load the UCF, without any change, and let me know if you still have the issue?
2026-04-07 3:25 AM
Hi,
Thanks again for your suggestion.
I implemented exactly the sequence “software reset → load UCF → no extra changes” on my ESP32‑S3 (Arduino, I²C, no libraries), but the MLC still does not start: EMB_FUNC_STATUS stays 0x00 and MLC0_SRC stays 0x00.
Code used
Wire.begin(5, 6);
// 2) Software reset
writeReg(0x12, 0x01); // CTRL3_C = 0x01
delay(100);
// 3) Enable embedded access
writeReg(0x01, 0x80); // FUNC_CFG_ACCESS = 0x80
// 4) Load UCF from Unico (Ac XX YY -> (reg,val) array)
load_mlc_config();
// 5) Disable embedded access
writeReg(0x01, 0x00); // FUNC_CFG_ACCESS = 0x00
In the loop I only read:
uint8_t emb_status = readReg(0x15); // EMB_FUNC_STATUS
uint8_t mlc0 = readReg(0x70); // MLC0_SRC
uint8_t is_mlc_ok = (emb_status >> 1) & 0x01; // tentative bit position
Serial output:
Start
UCF loaded
WHO_AM_I = 0x6C
EMB_FUNC_STATUS = 0x0 is_mlc_ok = 0 MLC0_src=0x0
So even with this minimal flow, is_mlc_ok never becomes 1 and MLC0_SRC is always 0x00.
After loading a valid UCF this way, should the MLC start automatically, or is there any additional enable step required outside the UCF?
Is the is_mlc_ok bit indeed in EMB_FUNC_STATUS as I am reading it, or should I check a different bit/register?
Does this behaviour point more to a configuration issue or could it indicate a possible hardware problem?
About my workflow, I currently generate the decision tree in Unico, and then export the .ucf that I send from the ESP32‑S3 with Arduino IDE. Could this conversion chain cause any issue for the MLC startup?
Would you recommend, for debugging, that I instead use DFU mode and only the official ST tools/evaluation environment to load and test the same UCF, to rule out any problem coming from my ESP32‑S3 + Arduino implementation?
Thanks again for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.