cancel
Showing results for 
Search instead for 
Did you mean: 

LPS28DFW511-LPS28DFWTR

MBENRiverkin
Associate

We are currently experiencing issues with the LPS28DFW.
We observe pressure values dropping to 0 or even negative ranges (e.g., around -400 mPa), as well as unexpectedly high values (up to approximately 1200 mPa), while the expected range should be around 950 mPa. We are also seeing abnormal temperature outputs, including unrealistically low values (e.g., around -400°C).

this happens when the sensor is in contact only with air and also when it is in contact only with water. When the sensors from the field they are brought back in the lab the sensors seem to recover on their own and return to normal readings.

1 REPLY 1
Federica Bossi
ST Employee

Hi @MBENRiverkin ,

It seems to be an issue with reading and interpreting data from sensor.
Please share your code and the sensor registers settings.

Thanks!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.