2019-10-09 9:25 PM
I was hoping that if there is some open-source software or STMicroelectronics based software in which I can send the serial data and that software could show the data in any graph format. Like, I need 4 windows on a single window, one for accelerometer, gyroscope, magnetometer, and for roll angle. There is software available by STM called X-NUCLEO but these are for only STM based MEMS sensor board. If you have any idea about this, please suggest.
Thank you.
2019-10-11 6:40 AM
Hi @Vivek Karna , do you simply need to plot graphically the LSM9DS1 data acquired with the STM32F411RE development board? If so, you could program a simple python or octave code and plot the graph on related GUI. If you can use the X-Nucleo based expansion board you can plot data with Unicleo-GUI tool. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.