2026-03-23 2:07 PM - last edited on 2026-03-23 2:20 PM by Andrew Neil
Hello ST Community,
I am currently in the hardware selection phase of a product development project and am evaluating STMicroelectronics accelerometers for our production design. I am hoping the community and ST engineers can help clarify driver availability and support options for our target platform.
Our production platform is based on the Quectel SC200U module running Android 14. The key processor specifications of this platform are as follows:
We are currently evaluating the following STMicroelectronics accelerometers:
1. Hexagon ADSP Driver Availability
Does STMicroelectronics currently provide Qualcomm Hexagon ADSP-compatible drivers for any of the following devices:LIS2HH12TR, LIS2DU12TR and LIS2DUX12TR. That are validated and compatible with Android 14 and the Qualcomm Hexagon ADSP framework?
2. Driver Access and Licensing If Hexagon ADSP-compatible drivers are available, are they available through an ST partner portal or Publicly accessible (e.g., via ST GitHub or official support channels)
3. Porting Guidance (If No ADSP Drivers Exist)
If no Hexagon ADSP-compatible drivers currently exist for these devices, what is the recommended approach for porting existing Linux kernel drivers to the Qualcomm Hexagon ADSP environment on Android 14? Specifically, we would appreciate guidance on:
Solved! Go to Solution.
2026-03-26 3:07 AM
2026-03-26 3:07 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.