MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FSM Github repository

I notice there is now a github repo with FSM examples; very useful!However, in comparing what I have been successfully using, for example, for shake detection on the LSM6DSV (or LSM6DSV80X) where 30 lines are written to page 0x7A: _i2c_bus->writeB...

KWine by Senior
  • 226 Views
  • 1 replies
  • 0 kudos

Resolved! How to program STEVAL-MKBOXPRO's audio buzzer?

In the getting started guide there is a programmable audio buzzer names SPK1 but I can't find reference of it anywhere, where I can enable it in the .ioc file and how to interact with it? Please could someone advise me on this.

nonayttd by Associate
  • 210 Views
  • 2 replies
  • 1 kudos

LSM6DSOX MLC Fails to Initialize - MLC0_SRC always 0x00

Hi, ST Community, I am working with an LSM6DSOX on a custom board, using an ESP32S3 with the Arduino framework, and I'm unable to get the Machine Learning Core (MLC) to run.The problem is that the output register MLC0_SRC (0x70) always reads 0x00. I ...

Resolved! CLI Example for Sensor Box Pro

The sensor box pro is a neat device.  If I use the CLI Example program and the USB cable, I can get 8000 data points per second, if I use a traditional C# program I get 8 data points per second.  The CLI yields dat files, which can be read with a sim...

LSM6DSV SFLP Setup with LPF1 and LPF2

 Dear all,I am struggling with getting a good SFLP result, that does not drift too much and does not appear jittery. I went trough most of the posts here but I am still not able to get good results (approx. factor 10 higher drift then according to th...

frabu_0-1774800084541.jpeg frabu_1-1774800084609.jpeg
frabu by Associate II
  • 392 Views
  • 2 replies
  • 0 kudos

LPS28DFW511-LPS28DFWTR

We are currently experiencing issues with the LPS28DFW.We observe pressure values dropping to 0 or even negative ranges (e.g., around -400 mPa), as well as unexpectedly high values (up to approximately 1200 mPa), while the expected range should be ar...

Resolved! MEMS Studio not working with ST1VAFE3BX

I've installed MEMS Studio v2.3.0 and trying to evaluate ST1VAFE3BX sensor -- in particular the vAFE ONLY operation in FIFO mode -- using the STEVAL-MKI109D evaluation board with STEVAL-MKI250KA evaluation kit plug-in module. Previously I had MEMS St...

bwilkins by Associate II
  • 406 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.