MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 FIFO usage when in 'Mode 1'/Slave-only

Posted on February 04, 2018 at 10:50For the &sharpLSM6DS3 - is it possible to use the &sharpFIFO also when the LSM6DS3 is in 'Mode 1'/Slave-only mode to buffer values of other sensor on the I2C bus? Or can the FIFO only be used when the LSM6DS3 is t...

Resolved! LIS2DW12 i2C communication issues

Posted on January 26, 2018 at 10:45Hi to all,We are usin this accel over i2c with this configuration:* Separate VDD and VDDIO (this one is attached to CS).* SDA and SCL are mounted with a external pull up resistor of 10K.* SDO/SA0 is left unconnecte...

IIS2DH Activity/Inactivity threshold setting

Posted on January 20, 2018 at 05:15Hi, I have configured accelerometer's registers as follows. So, from the activity threshold value how I know that at which raw value of X, Y, and Z axis it will be interrupted on a specific pin?////////////////////...

PIN outs for HTS221

Posted on January 28, 2018 at 06:52Is the pin out diagram on page 6 which is labeled ''bottom view'' actually a view from the top? VCC is in the upper left corner (pin 1).  The top side view shows the pin 1 ''dot'' also in the top left corner. and f...

0690X00000609VlQAI.png 0690X00000609W5QAI.png 0690X00000609VqQAI.png

LPS22HB is giving same value

Posted on January 22, 2018 at 09:27Hi I am using  LPS22HB with my custom made board based on STM32F777. I am reading LPS22HB using the same driver as ST is giving. I always read the same value of pressure i.e 1847. Temperature value is also incorrec...

Queru on LIS3DH sensor

Posted on January 24, 2018 at 09:54Hi,I am working on LIS3DH accelerometer sensor, I have interfaced this sensor with STM32F103 series micro controller using SPI interface. When I read X, Y and Z acceleration values, I get some random readings and i...

IIS2DH capacitors to VDD line

Posted on January 28, 2018 at 00:34Hello,Is it mandatory that 100nF and 10uF to the VDD line has to be ceramic and aluminium respectively?Also, we had three custom boards built with IIS2DH. Surprisingly, all three were giving a different XYZ values ...

Why is my INT1 of LIS2DW always at high?

Posted on January 25, 2018 at 18:52Hi,    My problem is I can not receive the interrupt signal of INT1 when I using FIFO mode with FIFO buffer full trigger. I find the cause is that the INT1 is always at high, but I expect it should be rise high whe...

0690X00000609UdQAI.png 0690X00000609UiQAI.png
Allen Lin by Associate II
  • 1340 Views
  • 1 replies
  • 0 kudos

LSM6DS3 Accel-Gyro Data problem

Posted on January 25, 2018 at 11:16Hi, i am using this sensor for a while now ,and i have a problem when i use together accelerometer and gyroscope. When i use them seperately everything works great, but if use both of them and acquire data from the...

Alex Dim by Associate II
  • 953 Views
  • 0 replies
  • 1 kudos

Data mismatching while Hard and soft reset

Posted on January 18, 2018 at 06:19Hello Miroslav, I have done following configuration for IIS2DH acceleromenter./////////////////////////// Sample Code ////////////////////////////////////////////////////response=LIS3DH_GetWHO_AM_I(&who_am_i); if(w...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.