2018-01-27 3:34 PM
Hello,
Is it mandatory that 100nF and 10uF to the VDD line has to be ceramic and aluminium respectively?
Also, we had three custom boards built with IIS2DH. Surprisingly, all three were giving a different XYZ values when kept in the same orientation. Please give me some suggestions as to what I have done wrong or in what I could do to mitigate this problem.
Thanks,
Ranjith
#iis2dh2018-01-27 4:16 PM
How different? Do you save any calibration data based on testing in a uniformly aligned test fixture? Do that parts lay flat on the PCB, and exactly the same orientation?
You want the bulk capacitor to have a low ESR so it can deliver instantaneous current without resistance. While the material/construction will impact the ESR, it is the ESR that should be the parameter used in the selection.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.