MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH low output registers outputting random data

Posted on March 30, 2018 at 18:51I have the LIS3DH accelerometer set for no FIFO, X,Y & Z output, Hi Res. I have BDU turned on.I am reading the high byte of each axis and getting the expected data which changes with accelerometer position. In all ca...

gbarbour by Associate III
  • 1138 Views
  • 2 replies
  • 0 kudos

lsm6dsl_reg.h possible error ?

Posted on April 01, 2018 at 17:28Hi, When using lsm6dsl_reg driver files I've stumbled on the following angular velocity conversion macros.The math seems wrong... Can ST verify this?Thanks#lsm6dsl_reg

LSM303DLHCTR - Peak Current Consumption Issue

Posted on April 02, 2018 at 19:18I'm using an LSM303DLHCTR in an application where I'm reading its X, Y and Z magnetometer values once per 20 ms, and have noticed that the chip seems to consume 10 mA or more of current from its 3.3V supply (VDD pin)...

HTS221 Cal. Coeficients

Posted on March 27, 2018 at 09:03Hello,I implemented the software for the HTS221 in my project and all is working. But what I find strange is this, some calibration coefficients are negative!H0_T0_OUT is -2H1_T0_OUT = -11728Although they are negativ...

LSM6DS3 Data ready Interrupt

Posted on March 27, 2018 at 09:13Hi, I`m facing a problem to get data ready interrupt on INT1.Use I2C communication.Trying to make fifo work and stuck with that, so started from data ready. According to Application notes :1 Write CTRL9_XL = 38h // A...

0690X00000604SiQAI.jpg

Voltage drop when connecting IKS01A2 to B-L072Z-LRWAN1

Posted on April 03, 2018 at 18:10So the B-L072Z-LRWAN1 board is configured to be powered through the 3.3V pin by removing SB6 and R26. Furthermore, the ST-LINK was disconnected by removing SB28, SB29 and SB37. When testing with some example code and...

How does LIS3DH configure automatic sleep and arousal?

Posted on March 16, 2018 at 11:40 I want to be able to when the device has detected movement, LIS3DH to wake up from sleep mode, and at a higher rate to detect more than I get a set of threshold, then the interrupt, to remind me of the MCU. I trie...

? ?_3 by Associate II
  • 4266 Views
  • 9 replies
  • 0 kudos

Resolved! Unable to get SensorTile working

Posted on March 04, 2018 at 10:22Hello,I have a SensorTile Kit (STLKT01V1) that I'm trying to test with the Blue MS Android application.As mentioned in the SensorTile http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/bc/b1...

MEMS (NIR)

Posted on March 31, 2018 at 18:39Hi I am currently working on a project with MEMS Sensors (Near Infrared Sensors between 1and 5 micrometer wavelenght), I am no Expert and my challenge is to evaluate user benefits and find application fields e.g. The...

LSM303C communication to microcontroller via 3-wire SPI

Posted on June 19, 2015 at 09:09I am interfacing LSM303C magnetometer and accelerometer to microcontroller via 3-wire SPI, where SIMO and SOMI from uC are connected together via R 10k to allow the slave LSM303C to drive this single signal line when ...

pljushev by Associate
  • 1472 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.