cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303DLHCTR - Peak Current Consumption Issue

Gary Sugar
Associate
Posted on April 02, 2018 at 19:18

I'm using an LSM303DLHCTR in an application where I'm reading its X, Y and Z magnetometer values once per 20 ms, and have noticed that the chip seems to consume 10 mA or more of current from its 3.3V supply (VDD pin) - for a short interval of about 4 ms during each 20 ms cycle - presumably while it's doing a magnetometer ADC conversion. The 10 mA is much higher than I expected, since the data sheet says to expect only 110 microamps of current draw. Accelerometer is disabled in my application. 

Has anyone else seen this behavior? 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on April 04, 2018 at 16:15

Yes, there are peaks on the Icc, they are typical for magnetometer operation.

The value 110uA written in datasheet is average value.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.