MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH Acceleration data calibration

Posted on May 04, 2018 at 11:11I am workeing with LIS3DH sensor ,Configured as normal mode with 2g .I am reading raw data please can any one help me to get the calibration of the X Y Z axesthanks

Resolved! LIS3DH temperature sensor when supply voltage is 1.8V

Posted on May 02, 2018 at 18:10Hello,I have a question regarding a note in the datasheet of the LIS3DH accelerometer:I want to use the accelerometer LIS3DH for one of my application with the following specifications:- The accelerometer is supplied a...

L CO by Associate
  • 1236 Views
  • 2 replies
  • 0 kudos

LIS3DH with strange output values

Posted on February 02, 2018 at 19:40Dear all,        For one important project i need to detect the human falls. I am using the LIS3DH accelerometer configured as the following manner:          CTRL_REG1=0x77 //ODR=400 Hz, high-resolution mode/norma...

magnetic rms noise of the LSM9DS1

Posted on April 16, 2018 at 23:37What is the magnetic rms noise of the LSM9DS1? I can not find it or something simular in the datasheet. Thanks for your help.#magnetic-rms-noise

Ralf L. by Associate
  • 1458 Views
  • 3 replies
  • 0 kudos

Accelerometer MEMS in various ''accelerometer'' chips

Posted on April 26, 2018 at 17:17Dear community,I was just wondering if there was any way of knowing (or whether this is 'secret recipe') whether the very-MEMS within different chips are the same or not.Namely, I would like to know whether I should ...

Operating VL53L1x in histogram mode

Posted on March 14, 2018 at 19:31Dear all,We are interested in reading out time-of-flight histograms from the VL53L1X to explore the application potential for SPAD technology for medical and cosmetic mass-market applications. The device appears to h...

VL53L1x - gesture recognition

Posted on April 26, 2018 at 08:11Hi,Anyone know how to config VL53L1x to gesture recognition? In datasheet is information about support 1D gesture recognition, but nowere I cannot find information how to config it to gesture recognition and how to u...

Maximum cover window for VL53L1X/VL53L0X

Posted on March 28, 2018 at 16:07The previous proximity sensor VL53L0X has a application note (AN4907: VL53L0X ranging module cover window guidelines) that specifies the cover window thickness limits for different distances that can be measured.I wo...

Resolved! Which Sensor should I use?

Posted on April 08, 2018 at 08:59I need a sensor that is able to differentiate between distance 20mm and 23mm with no error.i.e. the accuracy and stability must be high (within 1mm only)which sensor should I use VL6180 or VL53L or something else?

smhhadima by Associate II
  • 1312 Views
  • 1 replies
  • 0 kudos

VL53L1 underwater use / experiences?

Posted on April 24, 2018 at 13:46I understand the older vl6180x works underwater, but I could not find any information regarding the VL53L1. Anyone tried it? If so, how well does it work?I'm looking mainly for proximity detection / distance measurem...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.