2018-02-02 10:40 AM
Dear all,
For one important project i need to detect the human falls. I am using the LIS3DH accelerometer configured as the following manner:
CTRL_REG1=0x77 //ODR=400 Hz, high-resolution mode/normal mode, ZYX axis enabled
CTRL_REG2=0x01 // High pass filter enabled for AOI function on interrupt 1
CTRL_REG3=0x40 // IA1 interrupt on INT1
CTRL_REG4=0x84 // Output register not updated until MSB and LSB reading, high-resolution enabled
INT1_THS=0x20 // 16mgx32=0,512g
INT1_CFG=0x2A // Or combination of interrupt events. Enable interrupt generation on X, Y and Z high event.
When the accelerometer has just the gravity acceleration applied along the z-axis, the output registers OUT_X_L, OUT_X_H, OUT_Y_L, OUT_Y_H, OUT_Z_L have the value 0, the register OUT_Z_H has the value 255.
When i apply acceleration the output registers OUT_X_L,OUT_X_H,OUT_Y_L,OUT_Y_H,OUT_Z_L just assume one of the following values: 64;128,192. The register OUT_Z_H have always the value 255. Obviously the values should vary between 0 and 255. When i apply acceleration is generated one interrupt on the pin INT1 detected by one microcontroller. On attachment i send the values of the output registers and the calculated acceleration.
Any help will be very appreciated.
Best regards,
Rafael Costa
#lis3dh-with-strange-output-values2018-02-06 12:17 PM
From the screenshot I see the values for other output registers (except
OUT_Z_H) are always the same, which is strange. Is it like that? I suppose your reading procedure is not correct.
2018-02-07 1:41 AM
Dear Miroslav B,
My reading procedure was not correct. I want to read the output registers sequentially, but i forget to auto increment the address. To auto increment the address the MSB should be '1', as is explained on the section 6.1.1 of the datasheet.
Best regards,
Rafael Santos Costa
2018-05-03 11:57 PM
hi,I am workeing with lis3dh accelerometer please can u tell me how to calcuate the raw data to reading
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.