MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configure LIS2DH for both single click and double click

Posted on May 08, 2018 at 09:52Hello, I want to configure LIS2DH for generating interrupt for single click as well as double click, Can we do that? I am using INT1 for FIFO so INT2 is for clicks interrupt, Individually I can able to get interrupt fr...

X-CUBE-MEMS1 licence requirements?

Posted on May 08, 2018 at 02:56I started a project using the #osxMotionAR library which required a license from ST. This software has been moved into #X-CUBE-MEMS1 together with other osxMotionxx libraries. Is a software licence fro ST still require...

VL53L0X Time-of-Flight Distance Sensor ''FOV''?

Posted on April 11, 2018 at 09:45The specifications of the sensor states a 'FOV of 25 degrees'. I'm not really sure what that FOV means here. The beam is reflected back to the detector and filtered by a pinhole. There's a pinhole, so what would be t...

Resolved! VL53L0X Calibration Target - What to use?

Posted on March 24, 2018 at 14:24The user manual mentions using one 88% reflectance target and 17% reflectance target for calibration. I don't know what material has those reflectance values. What exactly should I use for calibration and where can I...

Josh Yu by Associate II
  • 4387 Views
  • 4 replies
  • 0 kudos

Is it possible to set minimum detectable range? VL53L0X

Posted on April 30, 2018 at 23:44Hi, Is it possible to set minimum detectable range for VL53L0X? I have an application with some parasitic reflections in 10cm zone which I want to ignore. Is it possible to set the detectable range for VL53L0X?

VL53L0X modifiy problem

Posted on April 12, 2018 at 16:25Hi there, I'm new at this form.I'm trying to use VL53L0X api with STM32F103VB cpu. But ı have a big problem. When ı try to use this api keil show windows.h include problem. When ı try this header to comment it sho...

github.com

Posted on April 25, 2018 at 19:02disappointing VL53L0x multiple sensors driver Hello,I got a st VL53L0X shield from ST, and for any people who needed some code, I wrote some faste code here:https://github.com/h2mille/les-beffroyables/tree/master/t%...

About VL53L0x

Posted on April 30, 2018 at 09:30Hi All,In my project, It has a cover above VL53L0x( about 5 cm). I want to know what kind of material that the VL53L0x will not to be disturbed by it.It means VL53L0x can work well when a cover above it.Thanks a lot....

VL6180X setting for specular/glossy reflecting targets?

Posted on May 07, 2018 at 12:05Hello,I have to perform some distance measurements in a system of stainless steel pipes. The VL6180X sensor I am using so far gives me values about 10mm below the true distance value.My assumption is that the non-diffu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.