MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Integrate IIS2MDC to STM32F103c

Hi,I am trying to read data from the IIS2MDC placed on a STEVAL-MKI185V1 on a STM32F103C board programmed via Arduino IDE. I tried following the steps mentioned in the document in the link:https://community.st.com/s/question/0D50X00009yDgrUSAS/is-the...

SBans by Associate
  • 2230 Views
  • 2 replies
  • 0 kudos

L3GD20H Motion Sensor

Hello,I am using the ​L3GD20H Motion Sensor for flight application and I need to compensate for temperature variation. There is a registry that I can read that provides a temperature value. Could you tell me what this value means and what it is refer...

PCote by Associate
  • 1456 Views
  • 3 replies
  • 0 kudos

Twait: LSM303CTR Why is there a Twait for IO pins and Vdd?

In the datasheet Twait was added to inform us to delay between powering up Vdd_IO and Vdd. However, the Twait timing says that there should be 0-10 mS wait period between Vdd-IO and Vdd. After waiting 0.1 - 100 ms Rise Time for Vdd-IO. What is the...

TSing.13 by Associate
  • 1015 Views
  • 1 replies
  • 0 kudos

Send MEMS-Mic-Audio to PC-Host

Hi, I try to connect a Nucleo-144-Board to Audacity. The Project is based on CubeMx5.2/STM32Cube_FW_L4_V1.14.0. I've read (successfully) in a Mems-Mic via SAI1/DMA2. The USB-Audio-Device is shown in the Device-Manager and seems to be OK. I've read th...

TTimm by Associate II
  • 1567 Views
  • 2 replies
  • 0 kudos

State Machine and stack size ?

Dear Members,I have a state machine but it seems that it stuck in one state,Is it related with stack size ?It's stuck on "case PULSE_IDLE" no matter the value of sensor_value,The code :switch(currentPulseDetectorState) { case PULSE_IDLE: ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.