2019-06-10 9:02 PM
Dear Members,
I have a state machine but it seems that it stuck in one state,
Is it related with stack size ?
It's stuck on "case PULSE_IDLE" no matter the value of sensor_value,
The code :
switch(currentPulseDetectorState)
{
case PULSE_IDLE:
if(sensor_value >= PULSE_MIN_THRESHOLD) {
//printf("Sensor_value PULSE_IDLE %f \r\n",sensor_value);
currentPulseDetectorState = PULSE_TRACE_UP;
values_went_down = 0;
printf("PULSE IDLE\r\n");
return true;
}
break;
case PULSE_TRACE_UP:
printf("Sensor value PULSE_TRACE_UP %f\r\n",sensor_value);
if(sensor_value > prev_sensor_value)
{
printf("PULSE TRACE_UP\r\n");
currentBeat =HAL_GetTick();
lastBeatThreshold = sensor_value;
}
else
{
printf("Peak reached: ");
printf("%f \r\n",sensor_value);
printf(" ");
printf("%f \r\n",prev_sensor_value);
uint32_t beatDuration = currentBeat - lastBeat;
lastBeat = currentBeat;
float rawBPM=0;
if(beatDuration > 0)
rawBPM = 60000.0 / (float)beatDuration;
printf("RawBPM = %f\r\n",rawBPM);
//This method sometimes glitches, it's better to go through whole moving average everytime
//IT's a neat idea to optimize the amount of work for moving avg. but while placing, removing finger it can screw up
//valuesBPMSum -= valuesBPM[bpmIndex];
//valuesBPM[bpmIndex] = rawBPM;
//valuesBPMSum += valuesBPM[bpmIndex];
valuesBPM[bpmIndex] = rawBPM;
valuesBPMSum = 0;
for(int i=0; i<PULSE_BPM_SAMPLE_SIZE; i++)
{
valuesBPMSum += valuesBPM[i];
}
bpmIndex++;
bpmIndex = bpmIndex % PULSE_BPM_SAMPLE_SIZE;
if(valuesBPMCount < PULSE_BPM_SAMPLE_SIZE)
valuesBPMCount++;
currentBPM = valuesBPMSum / valuesBPMCount;
printf("AVg. BPM: ");
printf("%f",currentBPM);
currentPulseDetectorState = PULSE_TRACE_DOWN;
return true;
}
break;
case PULSE_TRACE_DOWN:
if(sensor_value < prev_sensor_value)
{
values_went_down++;
}
if(sensor_value < PULSE_MIN_THRESHOLD)
{
currentPulseDetectorState = PULSE_IDLE;
}
break;
}
prev_sensor_value = sensor_value;Any clues on solving it ? thanks
2019-06-10 10:13 PM
Almost certrainly not.
With a stack problem, you would end up in the hardfault handler.
Perhaps your "sensor_value" is always less then PULSE_MIN_THRESHOLD ?
2019-06-10 11:15 PM
Data 7 Output MAX30100,0x09 register (FIFO DATA) IR : 1536
DC filterIR = -1147.117188
MeanDiff filterIR = 52967.000000
LowPass filterIR = 12989.482422
Timestamp After IRRED data= 25885
sensor_value > PULSE_MAX_THRESHOLD
Sensor_value PULSE_MAX_TRESHOLD 12989.482422
Sensor_value at PULSE_IDLE 12989.482422
PULSE IDLE
code :
switch(currentPulseDetectorState)
{
case PULSE_IDLE:
if(sensor_value >= PULSE_MIN_THRESHOLD) {
printf("Sensor_value at PULSE_IDLE %f \r\n",sensor_value);
values_went_down = 0;
printf("PULSE IDLE\r\n");
currentPulseDetectorState = PULSE_TRACE_UP;
//return currentPulseDetectorState = PULSE_TRACE_UP;
}
break;#define PULSE_MIN_THRESHOLD 300
I don't understand why ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.