2019-04-25 7:29 AM
I downloaded linux driver for LSM6DSL from official ST repositiory (https://github.com/STMicroelectronics/STMems_Linux_IIO_drivers/tree/linux-4.9.y-gh ) and seems that It works as expected.
One problem is that I can't find place where I can read temperature from OUT_TEMP_ register.
Is it somewhere hidden in IIO directory structures or this is not provided (most probably - based on sources) ?
Thanks
2019-06-07 4:00 AM
Hi, sorry for the delay in our answer, but did you try to read OUT_TEMP_L and OUT_TEMP_H (reg 20h and 21h) in the same way the data out of the LSM6DSL imu is read? Regards
2019-06-11 11:41 PM
Hi,
I managed to read temperature next day after my post :). I implemented this in similar way like reading of other properties.
I thought that this is independent temperature sensor but these registers returns 0 in case If there is no acc/gyro "data collection" enabled.
Anyway I was able to read temperature data but seems that it is not accurate enought.
In tests between -40 -> 85 I noticed following difference (compared to referance LM75)
Set: -40 LM75: -39 LSM: -48
0 0.5 -4
40 40 39
85 84 86
Right now it is not So much important for me So take this as a information only.
Regards
2019-06-12 12:12 AM
Hi, which temperature accuracy do you need? Please note that more accurate motion sensor + T feature will be soon released. Regards
2019-06-12 5:08 AM
Hi, Temperature itself (no acc/gyro samples).
LIke you can see on my previous email temperature values are different compared to onboard LM75 chip.
I saw difference up to 8 degrees on lower temperatures.
2019-06-12 6:07 AM
@Sigmoid please consider that the temperature is very dependent on the position on the board, especially if the motion sensor is nearer than LM75 t sensor reference to the more heat dissipating components (LDO, app processor...). Consider also that the T sensor embedded in LSM6DSL is not a precision sensor (the offset declared at datasheet is +-15°C!). Btw, a pretty new class of motion + T sensor with higher accuracy -comparable with LM75 one- is available (example here). Regards
2019-06-12 6:37 AM
Hi, I know all things that you mentioned here,
Thanks for suggestion.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.