MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3MDL Magnetometer Calibration

Hi, From what I've been told, the LIS3MDL magnetometers self-calibrate upon turning on. I have taken some readings from 3 different LIS3MDL's and plotted the values in a similar way to the beginning of this tutorial: https://thecavepearlproject.org/2...

0690X000008aEipQAE.png 0690X000008aEj4QAE.png 0690X000008aEklQAE.png 0690X000008aEkqQAE.png

How to derive the comparison limits for LSM6DS33 self-tests?

Regarding this thread:https://community.st.com/s/question/0D50X00009XkX2bSAF/lsm6ds33-problem-with-self-test?t=1558067735502The last comment by Petr says that the self-test values such as Min(ST_X) are derived from the Full Scale range, but he doesn'...

DAntl by Associate
  • 1425 Views
  • 1 replies
  • 0 kudos

does MotionFx library work in non ST MCU?

Our existing products are using NXP MCU and IMUs. We plan to switch to ST IMUs for the next generation, but still keep the existing nxp mcu. Is this possible? Can motionFX work in different mcu (m4f)? thanks!

lsm6dsl continuous mode with timestamps pattern unstable

Hi guysI configured the FIFO mode in LSM6DSL to extract the timestamps and Accel and gyrodata, and the data can be extracted properly. ​Since I now prefer to extract data consistently from the fifo for a long time, I switched to FIFO continuous mode...

jb by Associate II
  • 920 Views
  • 0 replies
  • 0 kudos

VL53L1X: temperature and repeatability

Hi friends,I want to measure the distance to an obstacle (120 mm) with the VL53L1X, but I am having problems with the repeatability.NOTE: I measure 10 times to get a sample and I repeat every 10 seconds.These are the results... The distance measured ...

0690X000008iFiFQAU.png 0690X000008iFmaQAE.png 0690X000008iFmfQAE.png

LSM303AGR Magnetometer interrupt occurs on ODR(10Hz) set instead it should occur on value changed beyond Threshold(100) set.Please see my magnetometer Register configurations

I have taken LSM303AGR Driver for development mentioned on this link: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm303agr_STdCI am getting issue of interrupt occurs at ODR time instead i require this interrupt should...

APate.19 by Associate II
  • 1191 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.