MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DSH SPI returning only 0s

I am working in a project with the LIS3DSH accelerometer. I have been working with it for some months and had no problems. void LIS3DSH_Class::enableAcc(byte _speed, byte _antialiasingFilter){ digitalWrite(CS_LIS3DSH, LOW); SPI1.transfer(CTRL_REG...

0690X000009jvXDQAY.jpg

Resolved! Long Blocking MotionFX_manger_run() Processing Time

Hi, I am currently having an issue where the MotionFX_manager_run Function is taking 4ms to process, blocking and starving other tasks. I am running at 48MHz on the STM32WB55 using the softfp compilation. How can I reduce the processing time of the f...

0690X00000AqWftQAF.jpg
Daniel L by Associate III
  • 1136 Views
  • 1 replies
  • 0 kudos

LIS2DH Interrupt for 6D movement detection

Hi,I am trying to make the interrupt work on the the Y-Axis, X-Axis, or Z-Axis.Here are the outputs I am getting. Threshold set to 960 mg. So when it gets bellow that threshold I am looking for an interrupt on the Z-axis. 0.280: Acceleration [mg]:14....

Tashfique by Associate II
  • 1422 Views
  • 1 replies
  • 0 kudos

Temperature sensors

Hi. Based on the temperature sensor i would also love to know ​what form of medium would be best for communicating the temperature to the microcontrollers, and their reasons. Thanks

NKenn by Associate
  • 939 Views
  • 1 replies
  • 0 kudos

Problems getting started with Sensor Tile

I am having a hard time getting started with the SensorTile and need some help. I am using CubeMx (v5.3.0) for the STM32L476JGYx selection, and observe the following result when I try to debug -Here is the error message:Here is the test setup:Thought...

0690X00000AppBWQAZ.png 0690X00000AppCKQAZ.jpg
Justin1 by Senior
  • 2538 Views
  • 4 replies
  • 0 kudos

Hi! I really need advice on what kind of a temperature sensor(contact type) would be perfect for sensing human temperature.

Hi! I am currently working on a project that involves the use of temperature of an individual to control a cooling system. I really need advice on what kind of temperature sensor(contact type) would be perfect for it. would really appreciate it if s...

NKenn by Associate
  • 1551 Views
  • 2 replies
  • 0 kudos

How to use UNICO with a custom MCU board?

I am trying to connect to a custom STM32L433-based development board (https://www.tindie.com/products/tleracorp/butterfly-stm32l433-development-board/) which is connected to an LSM6DSOX using UNICO, and while I can see the COM port in UNICO, when I t...

KWine by Senior
  • 895 Views
  • 1 replies
  • 0 kudos

LIS2DH12: 6d movement detection

I'm using LIS2DH12 and trying to implement 6d movement detection.Below is my present flow on startup.Set ODR to 25Hz in CTRL_REG1Enable i1_ia1 in CTRL_REG3Set full scale to 2g in CTRL_REG4Set aoi to 0 and remaining bits to 1 in INT1_CFGSet threshold ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.