2019-10-15 9:56 AM
Hi,
I am trying to make the interrupt work on the the Y-Axis, X-Axis, or Z-Axis.
Here are the outputs I am getting. Threshold set to 960 mg. So when it gets bellow that threshold I am looking for an interrupt on the Z-axis.
0.280: Acceleration [mg]:14.00 16.00 999.00
0.285: Temperature [degC]: 25.00
0.287: Int1 Threshold:0x3c
0.289: Int1 Configuration:0x50
0.291: Int1 Source:0x20
0.293: ctrl_reg3_t:0x40
0.155: Acceleration [mg]:-1027.00 -5.00 -39.00
0.160: Temperature [degC]: 25.00
0.162: Int1 Threshold:0x3c
0.164: Int1 Configuration:0x50
0.166: Int1 Source: 0x01
0.168: ctrl_reg3_t:0x40
set Ctr_reg_6 bit H_LACTIVE to 1.
The pin is constantly held low. If I set H_LACTIVE to 0 its constantly help high. I have configured pin 1 to detect a falling edge.
Maybe I am missing something.
Rest of the settings.
lis2dh_data_rate_set(&dev_ctx, LIS2DH_ODR_25Hz);
lis2dh_full_scale_set(&dev_ctx, LIS2DH_2g);
lis2dh_int1_gen_threshold_set(&dev_ctx, 0x12);
lis2dh_pin_int1_config_get(&dev_ctx, &ctrl_reg3);
ctrl_reg3.i1_ia1 = PROPERTY_ENABLE; lis2dh_pin_int1_config_set(&dev_ctx, &ctrl_reg3);
lis2dh_int1_gen_duration_set(&dev_ctx, 0);
_6d_cfg._6d = PROPERTY_ENABLE;
_6d_cfg.aoi = PROPERTY_DISABLE;
_6d_cfg.xlie = PROPERTY_DISABLE;
_6d_cfg.xhie = PROPERTY_DISABLE;
_6d_cfg.ylie = PROPERTY_DISABLE;
_6d_cfg.yhie = PROPERTY_DISABLE;
_6d_cfg.zlie = PROPERTY_ENABLE;
_6d_cfg.zhie = PROPERTY_DISABLE; lis2dh_int1_gen_conf_set(&dev_ctx, &_6d_cfg);
lis2dh_operating_mode_set(&dev_ctx, LIS2DH_HR_12bit);
lis2dh_pin_int2_config_get((ctrl_reg6_t*)®.byte);
reg.ctrl_reg6.int_polarity = PROPERTY_ENABLE;
lis2dh_pin_int2_config_set((ctrl_reg6_t*)®.byte);
2019-10-17 8:49 AM
I am getting an interrupt. But its all over the place ... Its not true to what the data sheet is saying. When I turn on orientation I get an interrupt in many directions. Is there any concrete example without polling..
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.