cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSOX is used. Is it possible to apply 3.3V to the VDDIO pin and 1.8V to the VDD pin? In that case, please tell me the current consumption of VDDIO and the current consumption of VDD.

KSait
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Eleon BORLINI
ST Employee

Hi @KSait​ , yes, the configuration you are using is allowed.

Considering the VddIO path, the current consumption basically depends from the device PD current consumption + the SPI contribution on the lines. This is around 100nA in case of VddIO 1.8V and 200nA in case of VddIO 3.3V.

On the other hand, the current consumption on VddIO path is directly related to the configurations and the settings of your device, and they are basically the data shown in LSM6DSOX datasheet.

Regards

Hi,Eleon BORLINI

​Thank you for your reply.

The current consumption when using 3.3V to VDDIO is about 200nA.

VDD is the current consumption described in the datasheet.

Best Regards

​Yes exactly, but please note that the faster the SPI, the more the VddIO line will consume more. So you can tune the SPI frequency (also according to your desired ODR) to optimize the current consumption. Regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.