MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH taking more than 100 uA

We are using LIS2DH in our board for production. Among 1000 boards, about 50 boards were drawing much more power because of LIS2DH (the IC is functional - we are getting the accelerometer data). Once we remove the IC from the board, current dropped f...

PK.1 by Associate II
  • 2964 Views
  • 7 replies
  • 0 kudos

Resolved! Cannot power down LIS3MDL

HI all,I cannot set sensor to power down mode.When i send command 0x03 to register CTRL_REG3, Current consumption is 100uA, i use stm8l151g6 (turn off hardware LIS3MDL current consumption is 1uA).

NPhuc by Associate II
  • 1080 Views
  • 1 replies
  • 0 kudos

Need soldering temperature profile for LIS2DE12

Hi, I am mounting the LIS2DE12 IC's using Infrared IC reflow machine using the profile having 257 °C peak. IC got soldered but, it is not detected, when I tried to communicate with it. I have tried for 3 IC's with same resulted. I suspect the t...

RKart by Associate
  • 1756 Views
  • 2 replies
  • 0 kudos

Dear Sir, How to connect Sensor tile cradle expansion board to PC and I tried with ST youtube video. But I unable to connect. My second question is I want to save the sensor tile Acceleration and Gyroscope data to the sd card. I requerst you suggest me

I want a 1000 data per seconds from LSM6DSM sensor (Acceleration and Gyroscope data ) and I want set acceleration level should +16g to -16g and gyroscope value should be 2000dps. These data should saved to the sd card. I request you to kindly sugges...

Problems calibrating VL53L0X ToF distance sensor (VL53L0X_perform_offset_calibration, VL53L0X_perform_xtalk_calibration). bug?

RoutineVL53L0X_perform_offset_calibration from src/core/src/vl53l0x_api_calibration.cpp is giving strange results. By my opinion the problem is in uint16_t sum_ranging which should be of type uint32_t due to later bit shifting (<<16), which needs to ...

GPodr.1 by Associate II
  • 892 Views
  • 0 replies
  • 0 kudos

multiple VL53L0x interfacig with atmega 2560

I want to interface 3 VL53L0x with atmega 2560 using arv-gcc and not arduino but i am unable to do so I have its documet but i dont understand how to implement please .Please help me to interfcae all sensor and read all of them at same time

AJHA.11 by Associate
  • 732 Views
  • 0 replies
  • 0 kudos

Bandwidth vs ODR

Hi,I would like to know what is the difference between bandwidth and ODR. I tough that just the analog accelerometers have bandwidth and the digital ones have ODR. For example, IIS3DWB can go up to 5kHz bandwidth and 26.7kHz ODR. Does this means that...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.