LSM6DS3TR-C thermal charactersitics.
Please share the below details for LSM6DS3TR-C,1. Junction to ambient thermal resistance?2. Junction to case thermal resistance?3. Maximum operating case temperature?4 .Maximum operating junction temperature?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Please share the below details for LSM6DS3TR-C,1. Junction to ambient thermal resistance?2. Junction to case thermal resistance?3. Maximum operating case temperature?4 .Maximum operating junction temperature?
Find the attached schematic and review the same.Here we are using I2C communication.CS pin is directly connected to the MCU
I am using the STEVAL-IDP005V1 and the terminal emulator, Putty, to output sensor data to my PC. I would like to plot the FFT data using Excel like is mentioned in page 20 of the Quick Start Guide. I have tried using the Putty configuration manager t...
Hi,I have a lsm6dsox sensor and everything is working fine, I can read the data and I can generate interrupts for single tap, double tap... But I want to configure as following:To set the sample rate at 52Hz, and every time it reads a sample to gener...
For example, given the following data taken from the sensor should the Y reading marked with a * account for a buffer overflow and therefore the difference be calculated as follows: 0xffff - 0xffd4 + 0x0e88 = 0x0eb3Initial X Reading: 0x0068Se...
Actually our device has 33 uA in DC current consumption without accelerometer LIS2DW12, with the LIS2DW12 this previous number increases to 55 uA.I think that it is possible to decrease the current consumption, based of the information of datasheets....
In the spec, Table 10 and Table 11 show's the current consumption when LIS2MDL working in different modes. But it doesn't verify the test voltage. Please help to confirm if they were measured in 2.5V. Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.