MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have problem with IKS01A2_LPS22HB_FIFOMode application generated by CubeMX. There are things in the code that i have to change.

I've generated project for SW4STM32 and i don't know that to do with iks01a2_conf_template.h file. Im supposed to replace the header file names with the ones of the target platform and rename the file to iks01a2_conf. There are 3 headers:#include "s...

CD.1 by Associate
  • 1136 Views
  • 1 replies
  • 0 kudos

Source code for ST.COM's X-CUBE-MEMS1 available?

Is the source code for ST.COM's X-CUBE-MEMS1available? I am using an STM32L412. And when I try to include the STM32 pre-compiled library into my project I get errors. I am thinking the processor I am using is not compatible with the libraries. So I...

Rstua.1 by Senior
  • 4075 Views
  • 9 replies
  • 0 kudos

How to connect more LSM303AH on one SPI BUS?

We are affraid when one device has CS signal down, other devices will be set to I2C there can be conflict on the SPI BUS. Is it possible connect more devices as eclosed schematic?

Using X-CUBE-MEMS1 for lsm9ds1

Hi, I want to use -CUBE-MEMS1 for lsm9ds1. By default the applications code uses LSM303AGR . Could any one give me some hints what changes I need to do for porting ECompas application for lsm9ds1. I have already ported the driver accelerometer, gyro...

Resolved! LIS2DH false positives in detection of clicks

Hello all,I am having an issue with single-click detection. I am getting false click detections at certain threshold values. I found this out yesterday when I had an MCU register lots of clicks repeatedly, but the device was not being shaken.To test,...

(LSM6DSL) how to get total G-Force

(Because I am not good at English, I used Google Translator.)​I'm using the LSM6DSL sensor now. I think that with this sensor still, the total gravity acceleration should be 1G, or 9.8.( Total - G - Force = SQRT(x^2 + y^2 + z^2 ) ) ​However, as the s...

Edoyo.1 by Associate
  • 1341 Views
  • 1 replies
  • 0 kudos

How to get MEMS board working with CubeMX?

Hi,I have just started my journey with STM products. I have STM32WB board with MEMS IKS01A3 extension board. I am trying to configure project using CubeMX software to generate code. I have created new project and added board extension IKS01A3, tunred...

LZure.old by Associate II
  • 1308 Views
  • 1 replies
  • 0 kudos

Hi, i need some help writing code of Heart Beat sensor max0100 I connected it to STM32L476 Discovery controller and activated the I2C pins in the STCUBE32IDE program. I dont know how to configure the MAX30100 in order to work with the controller

max 30100DataSheet - https://datasheets.maximintegrated.com/en/ds/MAX30100.pdfvideo explained the code for temprature sensor https://www.digikey.co.il/he/maker/projects/getting-started-with-stm32-i2c-example/ba8c2bfef2024654b5dd10012425fa23the contro...

YBuch.1 by Associate III
  • 2425 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.