2019-12-05 8:57 AM
I want a 1000 data per seconds from LSM6DSM sensor (Acceleration and Gyroscope data ) and I want set acceleration level should +16g to -16g and gyroscope value should be 2000dps. These data should saved to the sd card. I request you to kindly suggest me the procedure.
2019-12-16 8:44 AM
Hi @SKada.2086 , let's see the 1st question:
>> How to connect Sensor tile cradle expansion board to PC
Do you want to connect to the PC this board
or this one?
I suggest you to plug the SensorTile on this second board because in the 1st case you have to solder it and you could face difficulties
Regards
2019-12-22 10:46 AM
Dear Sir,
Thank you for your valuable reply.
In first case I soldered the sensor tile to cradle board and connected to mobile through Bluetooth by using the ST app and by default it is working from +2g to -2g and gyroscope data range is 1000dps. And also I am getting very less number of data ( 50 data per second).
I request you to kindly suggest me for the following queries.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.