Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Could anybody explain me about the purpose of GPIO that present in the sensor. How can we use that for an application, then there is a constant output voltage at range of 3v3 (when we give input voltage as 3v3 to sensor to work) is this voltage can b...
Hi,I'm acquiring gyros and accelerometers data through i2C bus, pulling the data from the FIFO asynchronously from the component acquisition frequency, but at a frequency close by (to avoid overfilling the FIFO).Without metrological tools, I can sti...
When the sample source code taken from STSTSW-STLKT01, the codes for the accelerometer is run and processed smoothly. However, the raw data and characteristics are not displayed in the nRF Connect app. No changes were made to the codes for the accele...
I have 2 LSM9DS1 9 axis chips and after waving them around I have the following min / max magnetometer values:chip1:X max/min: 657/-396Y max/min: 598/-417Z max/min: 377/-654chip2:X max/min: 533 -515Y max/min: 788/-284Z max/min: 0/-1213...that last Z...
I see that i2c operate up to 400Hz
Any ideas why LIS3DH is not consuming current as per data sheet which is 6uA whereas I am getting about 200uA.I have kept CTRL_REG0 at default.Would could be the problem?
I get an error when connecting to the board that the WHO_AM_I register value does not match the device selected. The correct device does appear in the Unico GUI menu (STEVAL-MKI206V1 (AIS2dw12). I also have updated my firmware today, the demo board f...
1 :i only use the Lis3dh ,and remove all other elements 2: i use the power 3.0V, i use multimeter test the current consume between VCC and GNDget the test result current is 16 μA,(the spec says ,the device automatically enters power-down mode, a...
Hello, I am simply tring to communicate with the L3GD20 Gyrosensor using the WhoAmI command. I am sending 0x0F and i'm expecting 0xD7 back (11010111) but I only received 0xFF which means i'm doing something wrongI am using STM32CubeMX to generate the...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.