MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MotionAR Initialize function gets stuck

Posted on January 24, 2018 at 17:10I am trying to add MotionAR library to a DataLogger sample application running on SensorTile. I manager to compile the library and program my chip with it. Near the top of my main() I added simple MotionAR_Initiali...

0690X00000609PBQAY.png
Norman S by Associate II
  • 2298 Views
  • 3 replies
  • 1 kudos

I'm want to acquire rawdata from the SensorTile.box (Steval$MKSBOX1V1). Using the app, I can get 16bits output raw data when Bluetooth streaming and then sending the files to email, but it's very limited.

How to I get control over the output data format? Is there a way I can upgrade the firmware, without any additional hardware (just using USB cable and STM32Cube IDE or Programmer) to change how I record the data?

MMarq.1 by Associate
  • 1924 Views
  • 3 replies
  • 0 kudos

how to configure threhold based interrupt in LPS25HB

hello,i m trying to  generate an interrupt event based on a defined threshold to wakeup the mcu from stop modehere is my function to enable this feature void LPS25_interrupt_Config(){   Conf_reg1 |= (LPS25HB_CTRL_REG1_PD | LPS25HB_CTRL_REG1_ODR...

ATAYE.1 by Associate II
  • 3567 Views
  • 7 replies
  • 0 kudos

problem with acceleration amplitude in IIS2DH

HelloWe tested the IIS2DH sensor on a shaker.Accelerometer Settings:ODR = 5376Full-scale = +/- 16gLow-power mode.High-pass filter bypassedShaker Settings:frequency 1 kHzacceleration amplitude 13.592 gAs a result, the accelerometer registered an accel...

ESmir.1 by Associate
  • 1434 Views
  • 2 replies
  • 0 kudos

IIS2DLPC Threshold Interrupt

Coming from the IIS2DH which had a simple threshold interrupt by axis that worked great. Can we achieve a similar thing with the IIS2DPLC? Specifically I want to do the following:If an axis exceeds a threshold value it will persist an output (INT1 or...

iaeinfach by Associate III
  • 1342 Views
  • 1 replies
  • 0 kudos

Hello! Can you let me know about the alignment error and bias instability terms of ISM330DLC model MEMS-IMUs? I have obtained the data sheet but I am not able to see these parameters I need. Thank you very much indeed!

We are making a market analysis on MEMS-IMUs in a private company and we would like to make fair comparisons between different IMU sets and we determined a few performance parameters for comparison. ISM330DLC is in our area of interest and we would l...

RAkta.1 by Associate II
  • 2589 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.