MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM9DS1 gyroscope interrupt threshold register

For LSM9DS1, what is the relationship between the interrupt threshold register INT_GEN_THS_X_G and the output register OUT_X_G?From the length of register, my expectations was that those two values shall have similar values (or factor 2).In my test, ...

ISoji by Associate
  • 564 Views
  • 0 replies
  • 0 kudos

How can I determine the value of the register ACT_DUR for a given ODR and a given desired return-to-sleep duration for LIS3DH?

In the data sheet, it is written: Sleep-to-wake, return-to-sleep duration 1 LSb = (8*1[LSb]+1)/ODR. How should I interpret that. It seems equation but is it? If one solves with respect to 1LSB, he/she would get: 1LSB = 1/(ODR-8) but it makes no sens...

IBuli.1 by Associate
  • 894 Views
  • 2 replies
  • 0 kudos

LIS2MDL Offset Cancellation Issues

I'm having trouble getting a heading from the LIS2MDL on our custom PCB. A summary of the issue:If in the presence of a strong magnetic field (ie. magnet), the LIS is able to report the field as expected and I can see headings calculated in the [-180...

0690X00000Bwgg9QAB.png 0690X00000Bwgg4QAB.png
Konami by Senior II
  • 1288 Views
  • 1 replies
  • 0 kudos

SensorTileBox identification problem with Windows 7

Hello, I have a steval-mksbox1v1 kit that I want to connect in Bluetooth with my pc in windows 7 but it doesn't work, I tested with windows 10 and it works fine, I don't understand the reason.Error indicated: "failed to add this device to this comput...

SAbid.2 by Associate II
  • 3119 Views
  • 6 replies
  • 0 kudos

How to connect STEVAL-MKSBOX1V1 using STLINKV3 to update firmware

I want to update the firmware of the STEVAL-MKSBOX1V1 to install the firmware I designed using AlgoBuilder. So I connect my STEVAL-MKSBOX1V1 to the STLINK V3 using 14 pin flat vable, and the STLINK to my pc using USB. Then I open cubeprogrammer and ...

NMart.1 by Associate III
  • 2254 Views
  • 4 replies
  • 0 kudos

Quaternions in AlgoBuilder with sensortile box

Hi everyone,I'm using the quaternions and the sensor fusion in Algobuilder with the Sensortile box in order to compare the signal of the quaternions and the position of the teapot, but I don't understand the relation between both of them... Any idea?...

LRoss.1 by Associate
  • 1200 Views
  • 1 replies
  • 0 kudos

H3LIS100DL sleep-to-wake - how to enable?

Greetings. I am familiar with the general sleep-to-wake functionality, I've used it successfully in the IIS2DH. However I am having issues with the H3LIS100DL. I believe I've enabled sleep-to-wake using control register 5, I've configured the interru...

cphelan by Associate II
  • 1746 Views
  • 2 replies
  • 0 kudos

How does Generic MQTT Cloud Logging work

Hi! I am using a SensorTile.box and tried to enable Generic MQTT Cloud Logging. Unfortunately I could not get any data to one of the public brokers. I used for example "tcp://mqtt.eclipse.org" Port 1883 (the tcp:// is mandatory, otherwise it won't wo...

DWind.1 by Associate III
  • 1635 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.