2020-03-19 7:35 AM
We are making a market analysis on MEMS-IMUs in a private company and we would like to make fair comparisons between different IMU sets and we determined a few performance parameters for comparison. ISM330DLC is in our area of interest and we would like to obtain this information.
2020-03-23 7:36 AM
Hi @RAkta.1 , with "alignment error" do you mean "cross axis error" (the fraction on x signal along y axis, for example) or non-linearity error? In this case, the cross axis value for the accelerometer is about 1% and for gyro is 1% too (data from characterization samples). About the bias instability parameter, the vale is 3deg/h, but always on the limited samples set of characterization tests.
For your interest, please let me tell you that most performing IMUs in ST portfolio are the devices of the LSM6DSOX family sensors. Regards
2020-03-23 8:02 AM
Thank you very much for the reply! With alignment error, I am referring to misalignment and cross axis error. Misalignment error corresponds to the deviation of the sensor triad with respect to the initial mount model, and the cross axis error is as you said, the correlation of each individual(x,y,z) on each other. Could you please enlight me with these parameters as well?
Best regards,
Rozerin.
2020-03-24 1:25 AM
Hi Rozerin, I have only available the gyro non-orthogonality, which is included in +-1% value on 6P. Regarding the mounting misalignment, its final value can depend also on the customer soldering process and has to be evaluated and compensated onboard in terms of offset compensation.
Btw, which parameters are included in the comparison you are performing among competitor IMUs? And for which application, if I can ask you? Regards
2020-03-24 3:05 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.