MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM9DS1 I2C Write to r/w registers

I have an LSM9DS1 IMU/Magnetometer and I am having difficulty in writing a value to the control registers and reading it back after.I am using the I2C protocol with my MCU device set up as the master and the LSM9DS1 setup as the slave.1.      I am ab...

JFand.1 by Associate
  • 981 Views
  • 1 replies
  • 0 kudos

IIS3DWB - How to configure for wake-up interrupt?

First i pull both interrupt pins to GND before power up the sensor, as recommended by the datasheet. I then configure SDO pin with pull-up using register PIN_CTRL. Then i enable the accelerometer with no second filtering stage from register CTRL1_XL....

TResell by Associate II
  • 1653 Views
  • 1 replies
  • 0 kudos

LIS2DH12 position of 6D.

I use LIS2DH12 to determine the position of 6D. My task is to get interruption when the accelerometer is positioned with the + X axis at an angle of 50 degrees or more. Autumn X is also disabled. In this case, the acceleration along the X axis = 1g. ...

AGari by Associate II
  • 2668 Views
  • 7 replies
  • 0 kudos

Some general info on the SensorTile.box (TileBox) required

So, i can operate the sensor box, install the updates a couple different ways and generally get it to work. But, the TileBox has three switches on board, none of which are accessible from the outside without adding some holes to the case. The TileB...

TJM by Senior II
  • 2204 Views
  • 5 replies
  • 0 kudos

LIS2DH 6D mode not working properly

Hello,I am trying to implement 6D mode. I am following 1:1 the code documented in the design tip DT0097.I have been trying for a while: I2C interface is working and other modes of LIS2DH work properly.As a safety measure, during the init I reset all ...

vcaia.1 by Associate II
  • 1906 Views
  • 6 replies
  • 0 kudos

MEMS Accelerometer application

HI Guys, I am looking for the MEMS Accelero meter for measuring the vibration in textile machines. Whether ST has the application example for condition monitoring system in machine or industrial automation.If so please share the details

NGopa.1 by Associate II
  • 2240 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.