MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hello, I'm currently testing the IIS3DWB accelerometer. The Datasheet says that the Timestamp tick resolution ist 25 us. All my measurements show, that the real resolution is 12.5 us. Is this correct?

This actually makes sense because the ODR is 26,667 kHz which means that between two samples are 37.5 us this would make three 12.5 us ticks. 25 us wouldn't make much sense.

MNoll.2 by Associate II
  • 2272 Views
  • 4 replies
  • 0 kudos

Question regarding implementation of LIS3DSH Standard C library.

Hi,I was taking a look at the STMems Standard C Library for the LIS3DSH. The implementation of the function lis3dsh_status_get looks a bit weird as there are 2 calls to the lis3dsh_write_reg functions.int32_t lis3dsh_status_get(stmdev_ctx_t *ctx, lis...

GTS.1 by Associate III
  • 2186 Views
  • 4 replies
  • 1 kudos

Resolved! Using INT2 on LIS3DSH for DRDY signal

Hi,I'm using a STM32F4 board which has a LIS3DSH. This board has PE0 connected to the INT1 of the LIS3DSH and PA0 connected to the user Button B1. Due to this, I won't be able to use interrupts to sample and interrupt for button press. I'm trying to...

GTS.1 by Associate III
  • 1835 Views
  • 3 replies
  • 0 kudos

Question from Predictive Maintenance Webinar 29th of April: Question on encryption hardware solutions and importance of secure TRNGs and QRNGs, see details section:

1) What are the current encryption hardware solutions based on which are used for designing PdM and CM applications? 2) How important is the use of cryptographically secure TRNGs or QRNGs for industrial IoT applications and what are the current hardw...

Question from Predictive Maintenance Webinar 29th of April: Can the STEVAL-BFA001V2B be interfaced with P-NUCLEO-IOM01M1?

Can the STEVAL-BFA001V2B be interfaced with P-NUCLEO-IOM01M1: STM32 Nucleo pack for IO-Link master with IO-Link v1.1 PHY and stack ? i choosed this second board because at the moment the STEVAL-IDP004V2 is not available at the moment from distitribut...

VL53L1X Low Temperature Performance

We using the VL53L1X in an application where it will be mounted in a manner that's protected from sunlight, but exposed to cold ambient temperatures - -40°C and possibly lower. The VL53L1X datasheet has a lower operational temperature limit of -20°C...

DAmer.1 by Associate
  • 1035 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.