MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-STWINKT1, any WiFi tutorials?

Is there any tutorials/AN for using the WiFi connectivity on the STWINKT1 board? What dashboard can i use to display sensor readings?

TResell by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

Resolved! Get factory settings/ firmware of the STEVAL-BCN002V1B

Hello,I have a question to the STEVAL-BCN002V1B. I try some BLE-Examples and flash the bord with some firmware example from the SDK. Now I can't pair the board with my mobile phone ST APP. Which firmware do I have to use to get the default factory s...

MMaie.1 by Associate II
  • 1776 Views
  • 2 replies
  • 0 kudos

壓力數值�?題

我�?�有購買STEVAL-MKI192V1開發�?��?�?LPS22HH的壓力感測器但使用上有一些�?題想請教 : 1. 壓力讀�?��?�?�為28H 29H 2AH, 溫度讀�?��?�?�為 2B 2C, 但壓力�?測出來的數值為35~FFH �?3EH�? 09H. 數值經�?�算�?符�?�壓力數值, 溫度也是相�?�的�??應.請�?�?如何解決 ?以上是10進�?顯示,由左至�?�分別為28H 29H 2AH資料​2. 本人是使用I2C通訊的方�?,請�?是�?�需�?�?始化...

0693W000001cE3nQAE.jpg
Dennis1 by Associate
  • 1037 Views
  • 1 replies
  • 0 kudos

ISM330xxx Library - Endianness problem

Hi,My setup:SP570S-DISP Demo Board EvaluationuC: SPC570S50E1IDE: SPC5Studio 5.8.1IMU Sensor: STEVAL-MKI207V1 (ISM330DHCX)I'm using "STMems_Standard_C_drivers/ism330dhcx_STdC" driver in order to manage communication between uC SPC570S50E1 and ISM330DH...

LeoC by Associate II
  • 2636 Views
  • 4 replies
  • 0 kudos

Resolved! Current consumption of LSM6DS3

Hi, I would like to know the current consumption of a LSM6DS3 with it's accelerometer and gyroscope running at 52 Hz and 104 Hz. The LSM6DS3 will be powered by a 2.8V source. Are there any official numbers or documents available for this?

GTS.1 by Associate III
  • 1324 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.