MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I easily combine the LSM6DS0 and the NUCLEO-L496-ZG?

In our current project, we chose a NUCLEO-L496 ZG as the core of our prototypes hardware. Now I am interested in combining the board with two fitting inertial measurement units. I think that the LSM6DS0 would be a good choice. How would you combine t...

MAlte.1 by Associate
  • 853 Views
  • 1 replies
  • 0 kudos

Hi, our designers are incorporating pressure sensor LPS22HH in to a product that requires post-assembly washing, prior to conformal coating. I can find very little information in the product literature relating to washing. Is this product washable?

Our standard washing process uses Vigon A201 chemistry at a 15% concentration in D.I. water. The washing solution is heated to 65 deg. C.Can anyone advise if this part is robust enough to withstand this process, perhaps if it has a post-washing bakin...

PBart.2 by Associate
  • 1862 Views
  • 2 replies
  • 0 kudos

ST Pedestrian Dead Reckoning Algorithm

Where can I find more info on ST Pedestrian Dead Reckoning Algorithm , I see a presentation from a past showcase, but nothing else. Anyone knows where I can get it, or who can I contact ?

EGarc.2 by Associate
  • 1847 Views
  • 2 replies
  • 0 kudos

I do not set the low power mode of the LIS3DH sensor properly.

I am using the ST LIS3DH sensor, and would like to try the low power operation mode, but the results I see on the display are not what I expected, since at rest, instead of seeing values of + -1g, I see values of + -3g, with a full scale of 2g.And I ...

EEstr.1 by Associate II
  • 3721 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.