Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
I have been using it already for a couple of weeks, today I plugged it in and I get that error. I tried to flash it again with the .bin file provided to update the firmware, but of course it's the same as previous version. I also checked the port num...
Hello,actually I am want to read data from fifo of the lis3dh sensor. I follow the datasheet and application note:write 00000000 in TEMP_CRG_REGwrite 00100111 in CTRL_REG1write 10001000 in CTRL_REG4write 01011110 in FIFO_CTRL_REGwrite 10000000 in CTR...
I have enabled the conditions needed to turn on the 6D orientation, and tried to read the registers according to these files: https://os.mbed.com/teams/ST/code/LSM6DSL//file/77ec4781b110/LSM6DSL_acc_gyro_driver.c/ and https://os.mbed.com/teams/ST/cod...
Hello ST-Community!When I'm using the LIS2DW12 at ODR=1.6kHz, the Interrupt for reaching the FIFO-Threshold is jittering with 1/ODR, but only if the threshold is greater than 12. If it's less or equal, everything is working fine.The buffer-Mode is se...
Hello,I am currently trying to implement offset calibration to VL53L0X sensor. I placed sensor in front of white paper with 100mm distance as datasheet suggest. When I get sensor measurement before offset calibration, I get 135mm which is fine becaus...
Hello,I am using LIS2DH12 with SPI connection. I am able to read back Device ID which is 51. Also, I can write a to the reference register and read back successfully. However, I cannot set registers. I am writing value on it and read back. The value ...
Hi,I am having uncertainties when calculating displacement and change of angle effected by random walk.I want to know proportion of failure in measurement caused by random walk.In the datasheet of ISM330DLC random walk (ug/sqrt(h) is declared as nois...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.