Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
I'm wondering if there are any concerns with acceleration measurement offsets and extra noise due to strain on the package from encapsulating it or potting it. I'm specifically looking at the LIS2DS12 if different packages have different answers to t...
Hi all,I did a firmware in python for LSM9DS1 and I red the register 0x18 with autoincrement but I noticed that there is a offset in gyroscope for axis x,y,z. So I did the single reading for the register but there is always an offset. How can I do t...
Hello Team ST, Sensor: LIS2DH12our application needs to detect motion activity. Since it is not time critical, we want to check this by reading the (latched) activity of INT2. I can see the motion activirty on th...
I am trying to update the firmware on my Sensor Tile Box (STEVAL-MKSBOX1V1). The current version on my Sensor Tile Box is 3.3.5. On startup, The IOS app indicates that the new firmware V3.41 is available for the box. However, trying to update to this...
I have been using MotionMC and I think it has been working. My compass appears to reach calibration as it starts working as expected and the calibration value reaches 3 (the highest level?).However, I've noticed while looking over my code that I am ...
I read AN4509.Single-axis tilt sensing is supported, but I can not tested it.1.Is Single-axis tilt sensing need gyroscope enable? Now gyroscope I disable it.2.Single-axis tilt sensing means I need disable other two-axis, remain only one sensing axis ...
Hi,I started working with LIS2DW12 trying to acquire simple data in pooling mode. I've done this wihtout any troubles using STM's mems drivers.Now, I'm trying to take this to a next level and I'm trying to work with LISDW12 FIFO's in interrupting mod...
Hello everyone,There is something I never understand about this type of project. In the project datasheet (X-CUBE-MEMSMIC1) as well as in many other projects I see this.Easy portablility across different MCU families ? What does that mean exactly ? s...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.