Temperature reading from LSM9DS1
When reading the temperature from a LSM9DS1, what's the unit that is used ? Cº ?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
When reading the temperature from a LSM9DS1, what's the unit that is used ? Cº ?
I've check this on the scope and everything on the I2C bus looks correct, I2Cwrite of 0x0F and then repeated start to read the value. Is there ever a case where it could return 0x33?Cheers
Is it possible to pass the telemetry data from one SensorTile to another to deliver the information from big distance like one kilometer ? As I understand the maximum range for BlueNRG-MS should be about 33 meters.Is it possible to make a chain of th...
Hello,I'm working with:NUCLEO-G070RBX-NUCLEO-IKS02A1STM32CubeMXSTM32CubeIDEIs there anywhere I can find the required STM32CubeMX settings to use the various X-CUBE-MEMS1 examples? I've downloaded everything in the last week so all the versions should...
I am working with the NUCLEO-F401RE board with the ST link connection and I have connected the SWD cables to the STEVAL GPT001V1 energy harvesting watch dev kit. I am following the user manual and it says I have to use this .bin file but I cannot fi...
Posted on June 20, 2018 at 17:39I've been beating my head against the wall for the last couple of days trying to figure out why I cannot read registers at odd addresses through the LIS3DSH SPI interface with the nRF52832. Byte accesses to even addr...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.