cancel
Showing results for 
Search instead for 
Did you mean: 

hello. I would like to measure the volume(or sensivity) of sound coming into a digital mems mic using ST's Audio IC. Is there any audio ic that can measure the volume (sensitivity) of the sound entering the mic among st products?

DSEO
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
DSEO
Associate II

i find a chip STA321MP now!

Is there any reference c-codes that I can refer to?

Eleon BORLINI
ST Employee

Hi @DSEO​ ,

the STA321MP audio amplifier is a good solution, but please note that the code available online uses the STM32 X-NUCLEO platforms for developing projects with MEMS microphones: the reference firmware function pack is X-CUBE-MEMSMIC1, and especially the function in \Middlewares\ST\STM32_Audio\Addons\SMR. This library is called Sound Meter, and is an optimized software implementation which embeds a pre-filter which can be configured with different filter types (A and C weighting, DC removal). It has also a smoothing filter which can be configured with any time constant value.

Please let me know if this solution can help your application development.

-Eleon

I had to unzip the file. (en.X-CUBE-MEMSMIC1.zip)

but SMR folder is not exist. (\Middlewares\ST\STM32_Audio\Addons\SMR )

it has only PDM floder

Hi @DSEO​ ,

maybe something has changed in the last function pack version... you can however find the same directory in the standard X-CUBE-MEMS1 firmware package, folder \Middlewares\ST\STM32_Audio\Addons\SMR.

You can find the application that uses this library in \Projects\STM32L476RG-Nucleo\Applications\IKS02A1\SoundMeter. This is platform dependent, based on STM32L476RG-Nucleo board (but you can use other Nucleo motherboards), and on X-NUCLEO-IKS02A1, that is equipped by theST IMP34DT05 MEMS digital microphone.

Let me please know if you succeed in using it in your code.

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.