MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Regarding imp34dt05 mems sensor configuration

Sir,I am working on the imp34dt05 sensor but how could we configure its parameter.Could u guide us for that.What should be sampling frequency and what is the range of the frequency that it can capture and what should be sampling frequency of pcm and ...

Ultra Low Power Mode for LSM6DS032 is not working.

Currently designing a  low power embedded system for monitoring application using IMU LSM6DS032, tried both low power/normal mode and the ultra low power mode setting on this IMU, but I could not find the significant difference in the power consumpti...

Resolved! IMU layout for flex PCB

I am reading through TN0018 and saw that it is possible to have signal and plane on the bottom layer. Does this apply to flex PCB with 50-150um thickness? 

qkieu_0-1754420772882.png
qkieu by Associate
  • 834 Views
  • 1 replies
  • 0 kudos

ASM330LHH - large gyro biases

Hello, We are using the ASM330LHH in a design and are seeing extremely large gyro biases (~250 deg/s). I am trying to figure out what may be causing them; here is some information on the experiment. We collect data while spinning our custom boards (w...

rcoman_3-1754069871175.png rcoman_2-1754069782871.png
rcoman by Associate
  • 495 Views
  • 1 replies
  • 0 kudos

Interfacing MP34DT06 with STM32F401RE Sensor

Hi,I’m using the NUCLEO-STM32F401RE with the X-NUCLEO-CCA02M2 board, which has two MP34DT06 PDM microphones. I want to capture stereo audio using I2S2 and convert it to PCM using the PDM2PCM middleware in STM32CubeIDE.In AN5027 (page 18), a timer is ...

impacts of IIC error injection with IIS2DLPC

For special test case, that directed connected IIC's SCL(LUX_TILT_SCL) to GND and kept for 5mins, will this action hurt or damage IIS2DLPC?IIC worked with 100kbps.Work with IIC. We found that after this action/error injection:Sometimes, the sensor ca...

BBBBBB_0-1753955870719.png
BBBBBB by Associate II
  • 953 Views
  • 6 replies
  • 3 kudos

IIS2ICLX inclination

Hello, I'm looking for a very high precision inclination sensor. I found this IIS2ICLX. I have some questions on the specifications.1) What is the repeatability of the device?2) From the spec sheet, it might seem like the repeatability of the device ...

gio926 by Associate
  • 1395 Views
  • 2 replies
  • 0 kudos

Reading ISM330DHCX with Nucleo Board (SPI3)

Hi,I am trying to read data from my ISM330DHCX using my STM32G491 Nucleo board over SPI3However, I am having trouble understanding the operation of this device, so I would like to explore the answers to the following questions:1) What is the most bas...

Matthew47_1-1753880655726.png

Resolved! Accelerometers comparison

Dear community,I am selecting an accelerometer to use in a project and I am looking for some advice.Essentially I am looking for the highest performance accelerometer (regarding noise) in the STM portfolio.The sensor requirements are: ~±2g scale supp...

dburgt98 by Associate II
  • 5067 Views
  • 10 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.