MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Check configuration on lsm6dso32

Hi! I inherited a project and we're seeing strange accelerometer values and I'd like to get a sanity check on my configuration. when Idle and flat, I see 1g on Z, 0g on X and Y. When my device is moving I see peaks on many axes beyond 1g, eg 2.5 on X...

ms360_0-1753746022179.png
ms360 by Associate II
  • 777 Views
  • 4 replies
  • 0 kudos

LIS3DH Double interrupts detection

Hi ST guys,I played with the LIS3DH accelerometer options and don't really see difference in interrupts.Can you explain the differences between 6D and no 6D because as per my understanding of AN3308 the AOI + 6D option is position detection which is ...

quick691 by Associate
  • 504 Views
  • 0 replies
  • 0 kudos

Resolved! X-NUCLEO IKS4A1 with STEVAL-MKI212V1 (ASM330LHHX) DIL24

Hello!!I just started with the ASM330LHHX DIL24 module for the X-NUCLEO Boards, the module is listed as compatible with the IKS4A1 (sensors below):I have read some documents related to the procedure to make it work but it's an "old" document (see bel...

Pantera_MXJ_0-1752821592794.png

Resolved! MEMS studio Data Monitor bug

Hi,  I'm struggling to monitor the debugging values on the MEMS studio. setup1. MEMS studio 2.1.1 (latest version)2. Sensor PRO Tile Box + STEVAL-MKI229A(LSM6DSO16IS)3. ST Official ispu-example GitHub, normhttps://github.com/STMicroelectronics/ispu-e...

Screenshot 2025-07-26 at 12.45.33 AM.png Screenshot 2025-07-26 at 12.44.11 AM.png
seopp by Associate
  • 463 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-FCU001V2

I'm new to the STEVAL-DRONE2 kit and would like to ask: Given that the STEVAL-FCU001V2 flight control unit includes basic sensors like the IMU and barometer, can it support the integration of additional external sensors, such as GPS modules, magnetom...

sani-k by Associate
  • 761 Views
  • 2 replies
  • 0 kudos

Resolved! Three qestions about MotionFX CM0+

Hello wonderfull STM community,Really enjoying the experience with MotionFX so far, really easy to implement and get working, well done ST! Even on a G0 in CM0+ mode its working well! I'm just woudring three things:What precaution(s), if any, should ...

WrenchInTheWorks_0-1752136756774.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.