MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to clear LSM6DSOX I3C IBI interrupt status?

I'm now using LSM6DSOX with I3C protocol. And I'm trying to use ibi to notify a tap event. Here are the following information to configure the sensor register: LSM6DSOX_INT1 0x0D 0x00LSM6DSOX_INT2 0x0E 0x00LSM6DSOX_CTRL1_XL 0x10 0x3CLSM6DSOX_CTRL2_G ...

simon_myth_2-1755844500271.png simon_myth_0-1755844395670.png simon_myth_1-1755844436494.png

Filltering on CCA02M2

Hey ST Community,I'm currently trying out the CCA02M2 MEMS microphone board on a NUCLEO-L476RG, using firmware compiled from X-CUBE-MEMSMIC1.The microphones work, but the signal seems to have some heavy filtering. For example:If I record with Audacit...

KRT by Associate
  • 727 Views
  • 0 replies
  • 0 kudos

How to get calibration level for IMU sensor and magnetometer

After soldering process, IMU sensor and magnetometer need to do calibration after power on, such as flip axis, 8 shaped pattern, or real-time calibration.For ST sensor such as LSM6DSV and LIS2MDL, I want to know how to confirm whether sensor has been...

Yansu by Associate III
  • 3553 Views
  • 4 replies
  • 0 kudos

Actual Detection Range and FOV of STHS34PF80?

Hello everyone,I’ve been working with the STHS34PF80 sensor and would appreciate some insights regarding its detection range and field of view (FOV). In my tests, I’ve observed that the sensor detects presence effectively up to a range of about 1 met...

mobaid by Associate II
  • 2005 Views
  • 3 replies
  • 0 kudos

STHS34PF80

I am using the STHS34PF80 sensor (SparkFun Presence Sensor - STHS34PF80) with an ESP32 in my ceiling fan to automatically turn the fan ON and OFF based on human presence and motion. However, the sensor is providing continuously varying output values ...

Compatibility STEVAL-MKI227KA Arduino Mirco

Hello,I'm working on an IMU project. I need to measure pitch/roll/yaw rotation in quaternions.For my first test, I am using a STEVAL-MKI227KA connected to an Arduino micro, which already allows me to extract the quaternions.I send the data via I²C.My...

BapDBD by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

Sensortile.box Pro fails verification after programming

Hello,I was having fun with the Sensortile.box Pro I bought a month ago. When I reset the device to its factory settings (SensorTile.boxPRO.bin in file en.stsw-mkboxpro-fs.zip) using the STM32CubeProgramming tool, the device blinks the red LED once a...

cookao by Associate II
  • 6975 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.