MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MotionFX magnetometer calibration not always working

Hi everybody,I use the motionFX with accelerometer, gyroscope and magnetometer (9X sensor fusion) but I have a problem using the magnetometer calibration.I proceed as mentioned in the documentation of motionFX library:Call MotionFX_MagCal_initCall Mo...

BFlor.1 by Associate II
  • 2652 Views
  • 4 replies
  • 0 kudos

Resolved! Set H3LIS331DL to generate continuously Pulse for DataReady Interrupt

Is it really possible to configure H3LIS331DL to fire an interrupt (a pulse) for each DataReady ?I've never succeded in doing that, It seems to be always mandatory to read Acceleration to "release" the interrupt line, hence being able to have a new i...

PGoud by Associate III
  • 3110 Views
  • 4 replies
  • 0 kudos

Resolved! LIS2DW12 and nRF52840 Feather Express via I2C HW issue

I have a simple setup of (Arduino) nRF52840 Feather Express connected to steval-mkiv1-184872 -evaluation board. I was going to use it via I2C bus, and followed the connection diagram almost to last letter.   I connected SDA/SCL to feather   I connect...

I have lsm6dso sensor. I am using fsm interrupt for different events. I have 3 programs in fsm. When the event detected, interrupt comes.I gave three fsm program to same interrupt pin. But I want to know which fsm event detected ?

I have lsm6dso sensor. I am using fsm interrupt for different events. I have 3 programs in fsm. When the event detected, interrupt comes.I gave three fsm program to same interrupt pin. But I want to know which fsm interrupt detected .When I read the ...

Iakgu.1 by Associate III
  • 3306 Views
  • 6 replies
  • 0 kudos

Resolved! STTS22H - I2C Address Setting

Hello,In the data sheet of the sensor (https://www.st.com/resource/en/datasheet/stts22h.pdf), it's mentioned that to set the Address we need to connect the ADDR pin whether to VDD (to have the address 0111000) or to GND (to have the address 0111111),...

OHADD.1 by Associate
  • 2476 Views
  • 3 replies
  • 0 kudos

Resolved! lsm6dso fsm filter

I have lsm6dso imu sensor, I can add high pass filter or slope filter for wake-up interrupt.Is it possible to add filter to fsm interrupt ?

Iakgu.1 by Associate III
  • 2778 Views
  • 4 replies
  • 0 kudos

LSM6DSO FIFO Timestamp Gets Reset After 0xFFFF

Any ideas on why the timestamp gets reset in FIFO after 0xFFFF? I have TIMESTAMP_EN bit of theCTRL10_C register set to 1 and the DEC_TS_BATCH_[1:0] bits of the FIFO_CTRL4 are set to 01 (max(BDR_XL[Hz],BDR_GY[Hz]) [Hz]).

BDiva.1 by Associate II
  • 1085 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.