2021-04-13 1:13 PM
Any ideas on why the timestamp gets reset in FIFO after 0xFFFF? I have TIMESTAMP_EN bit of the
CTRL10_C register set to 1 and the DEC_TS_BATCH_[1:0] bits of the FIFO_CTRL4 are set to 01 (max(BDR_XL[Hz],BDR_GY[Hz]) [Hz]).
2021-04-14 1:08 AM
Hi @BDiva.1 ,
there are two reason for which the timestamp can reset:
you wrote that it resets after 0xFFFF, but what register are you reading? is it TIMESTAMP 0 and 1, or 2 and 3?
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.