MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How is marked IIS3DWBTR?

Hi Community,We send to manufacturing PCB to our supplier but he has a problem with the mark(attached) of the sensor IIS3DWBTR, and we want know if the brand is correct for component, we try to read the image as Qr Code and result is 780270TU01RY, bu...

MSierraA by Associate II
  • 5650 Views
  • 9 replies
  • 1 kudos

VL53L1X SetAddress after device disconnected

Hi,I use 4 VL53L1X sensor with an arduino and ULD API. I set the address on 0x31, 0x33, 0x35 and 0x37..I try to prevent a critical case which appear when one or more device are lost (timeout or hardware disconnection).To do so, I intercept the lost o...

OTELL.1 by Associate
  • 1294 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DH, bad pin configuration?

Dear ST member,I attached a piece of my schematics design. Can LIS2DH works with pins 3 (SA0) and 4 (CS) not connected?Regards

0693W000008zEnmQAE.jpg
jartigas by Associate II
  • 1125 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F103xC and LM35 wrong readings

Hey, I'm trying to get some temperature readings from LM35 sensor and I'm using "blue pill" for this little project and of course ADC. The problem is that I am getting wrong readings, approximately half of the real value. I know that the sensor is go...

DSimp.1 by Associate III
  • 3606 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.