2024-09-11 5:43 AM - edited 2024-09-11 5:55 AM
Hello everyone,
I’ve been working with the STHS34PF80 sensor and would appreciate some insights regarding its detection range and field of view (FOV). In my tests, I’ve observed that the sensor detects presence effectively up to a range of about 1 meter when I set the presence threshold to 100 LSB. Additionally, the FOV seems to be around 30 degrees.
I’m wondering if these results align with what others have experienced. Is this the typical range and FOV for this sensor under similar conditions, or could there be some optimization or calibration that I’m missing? Any feedback or suggestions would be greatly appreciated!
Thanks in advance!
Note
sensor config:
lpf_m: 04, lpf_p: 04, lpf_p_m: 02, lpf_a_t: 00
sths34pf80_gain_mode_get 7
sths34pf80_tobject_sensitivity_get 2000
sths34pf80_odr_get 8
sths34pf80_block_data_update_get 1
sths34pf80_one_shot_get 0
sths34pf80_presence_abs_value_get 1
sths34pf80_tobject_algo_compensation_get 1
sths34pf80_presence_hysteresis_get 25
sths34pf80_motion_hysteresis_get 25
sths34pf80_tambient_shock_threshold_get 10
sths34pf80_motion_threshold_get 100
sths34pf80_presence_threshold_get 150
2024-09-20 2:59 AM
Hi @mobaid ,
We see no problem in the used configuration.
The expected FOV and detection range are much larger.
Can you give us more information about the test environment and conditions?
2024-09-22 7:05 AM
Hi @Federica Bossi ,
Here are the test environment conditions :
T ambient | 23’C ~ 25’C (Air conditioner) |
Application | Indoor office |
Sensor to Wall distance | 3m |
Sensor Hight | 1m |
Lens | N/A |
AVG_TMOS : Number of averaged samples for object temperature | 32 |
AVG_T : Number of averaged samples for ambient temperature | 8 |
Interrupt source | Presence |
Presence and motion detection setting | |
Presence threshold | 150 |
Presence hysteresis | 25 |
Motion threshold | 100 |
Motion hysteresis | 25 |
Thank you .
2025-08-17 11:55 PM
Subject: STHS34PF80 Sensor — Inconsistent Output with ESP32 and SparkFun Library
I am using the STHS34PF80 sensor (SparkFun Presence Sensor - STHS34PF80) with an ESP32 in my ceiling fan to automatically turn the fan ON and OFF based on human presence and motion. I’m using the official SparkFun library to read the sensor values.
However, I’m noticing inconsistent readings:
Sometimes the sensor gives values above 1000 when a person is around 60–70 cm away.
Other times, under the same conditions, it gives 0 or even negative values.
I would like to know:
How can I configure the sensor for more reliable presence detection?
Does the sensor have a refresh rate, integration time, or filtering option that needs adjustment in code?
Any guidance on how to stabilize or interpret the sensor output would be appreciated.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.