MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12 WrongTemperature readings

I am working on the LIS2DH12 chip for accelerometer and temperature readings. I am facing an issue with the temperature readings. Please find below the steps for reading the temperature value.Sensor Initialization for Temperature :1. Initialization o...

Cannot get the Data Ready Interrupt working on the LIS2DE12TR.

We really need help getting the LIS2DE12TR to toggle the INT1 pin when new data is ready to be read. I've included the workspace bundle of our source. We are using a Cypress microprocessor.We can read the Whoami and successfully get 0x33.We've writte...

PDavi.5 by Associate
  • 1031 Views
  • 1 replies
  • 0 kudos

Resolved! L3GD20H wrong gyroscope readings

I'm using L3GD20H on a flight controller board for drones.While conducting a temperature test that starts from -11°C and ends at 50°C, I observed a sharp rise/drop in gyro values at around 23°C. (The board stayed still the whole time inside a vibrati...

0693W000008wTuaQAE.png 0693W000008wTuVQAU.jpg
Gabsu by Associate II
  • 3426 Views
  • 9 replies
  • 0 kudos

MPU6050 gyroscope x and y axis data not right

I have collected 200 samples of the gyroscope raw data and get the average to calculate the offset. After that, I leave the sensor on table and try to read the raw data. The raw data read should be close to the average value that I obtained at the be...

0693W00000Bc2MEQAZ.png
M7890.1 by Associate III
  • 2911 Views
  • 4 replies
  • 0 kudos

Hello, I'm trying to import in my workspace a demonstration project provided by ST in X-CUBE-MEMSMIC1 and I get the error message below. How can I fix it? Thank you

Problem running CDT Scanner Discovery provider com.st.stm32cube.ide.mcu.toolchain.armnone.setup.CrossBuiltinSpecsDetectorError serializing language settingsInternal error while trying to serialize language settingsCannot create file, access denied: C...

MSant.11 by Associate III
  • 1415 Views
  • 3 replies
  • 0 kudos

Connectivity problems between SensorTile.box and Matlab

I'm trying to establish the connection between the SensorTile.box and Matlab. When I search for the Sensortile.box with the proper Matlab command, I can see the device but then, when I try connecting it, I get an error. I tried the same with a Sensor...

MFilo.1 by Associate
  • 908 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.