MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to reset sensortile Box ?

I flashed my sensortile box but it stopped working after that. ( no lights blinking ).I did a reset on it using STM PRG. But still even when i plug it in still no lights are blinking. Battery is connected but there is no light.

AMuee.1 by Associate
  • 1238 Views
  • 1 replies
  • 0 kudos

Resolved! implement tap detection using Lis2hh12

I want to implement double tap detection using LIS2HH12 accelerometer. It does not have in-built registers to implement it. Has anybody implemented it?

SK.16 by Associate II
  • 3118 Views
  • 4 replies
  • 0 kudos

Accelerometer with vector-magnitude change event detection

Hi,I would like to ask you, do you have accelerometer with vector-magnitude change event detection with programmable reference, threshold, anddebounce time values ?I need to detect accelerometer orientation change, but not from 0g but for example fro...

Resolved! Calibration Values LSM6DS33/LSM9DS1

Hello everyoneI'm currently working on a research project concerning IMUs, among others a LSM6DS33 and a LSM9DS1 module. In the datasheet for the LSM6DS33 and LSM9DS1 a factory calibration is mentioned (e.g. bottom of page 40). Since nothing else is ...

NSeid.1 by Associate
  • 2834 Views
  • 3 replies
  • 0 kudos

Teseo GNSS module - no fix

Hi, I have own design with Teseo GNSS LV3R module. It is connected to STM32L071. After power up I just set Reset pin to low for 10 ms and then I keep it in high level. Unfortunatelly even after 3 hours under open air ( without clouds and nearby build...

0693W00000BaDOMQA3.png 0693W00000BaDOHQA3.png
JJRR by Senior
  • 2245 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.