MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am trying to deploy dsh-predmnt to my personal aws account but serverless is throwing a lot of errors. I followed the PDF document "How to deploy DSH-PREDMNT in proprietary AWS account" . Is there a more detailed instruction on deploying to AWS??

PS C:\pm\predictive_maintenance_fe\serverless>node --versionv14.16.1PS C:\pm\predictive_maintenance_fe\serverless>npm --version7.11.1PS C:\pm\predictive_maintenance_fe\serverless>npm install   up to date, audited 190 packages in 2s   6 packages are l...

VChak.1 by Associate II
  • 4764 Views
  • 8 replies
  • 1 kudos

Resolved! ST BLE Sensor App and Dashboard - Offline.

I've the STEVAL-STWINKT1B,I've flashed ,\STMicro\SW\en.fp-sns-datalog1\STM32CubeFunctionPack_DATALOG1_V1.1.0\Projects\STM32L4R9ZI-STWIN\Applications\HSDatalog\Binary/HSDatalog.binBut I do not able to read the sensor data.I do not access the environme...

LK N.1 by Associate II
  • 3823 Views
  • 11 replies
  • 0 kudos

LIS25BA TDM interface restrictions

HiI am trying to add LIS25BA to be used under TDM along with another device. I have found that LIS25BA datasheet and LIS25BA application note are not match accurately. Could you please help me understand following moments:Datasheet (chapter 4.2):The ...

DRodi.1 by Associate
  • 1734 Views
  • 2 replies
  • 0 kudos

Resolved! H3LIS100DL I2C ISSUE

I am Working on H3LIS10DL And i have Read The WHO_AM_I Id of the H3LIS100DL i got the WHO_AM_I id is 32h. But not getting Correct Data of X,Y,Z Axis Also i Have tried the ST Library for the H3LIS100DL but seems we are not getting the correct data on...

Ajeth.11 by Associate III
  • 5656 Views
  • 2 replies
  • 0 kudos

Resolved! New project generates incorrect IOC file

Hi all,I created a new STM32 project using File->New->STM32 Project in STM32CudeIDE and selecting the STWINKT1 board. It produces an .ioc file that shows quite some warnings in the Pinout & Configuration tab of the Device Configuration Tool. It also...

I am using the IISDWB and am trying to configure it for FIFO mode. FIFO_STATUS2 is always returning 0x6A signaling that FIFO in going into overrun. Any ideas why this is constantly happening?

I read FIFO_STATUS 2 within main, then execute a for loop that will read all bytes stored in FIFO (as per the DIFF_FIFO_BITS : (DIFF_FIFO_BITS are always reading 0x200 as a result of this error with FIFO_STATUS2). And I make sure to read 7 bytes at ...

SSedi.1 by Associate II
  • 1950 Views
  • 7 replies
  • 0 kudos

Resolved! How to make SensorTile.box discoverable again?

Hello, all.So I have this problem with my SensorTile.box. I received it this afternoon, and I connected it to my desktop PC via a USB cable while the PC was starting. It shows up on the device list on the ST BLE Sensor app; the device's red light wa...

JGonz.10 by Associate
  • 1047 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.