Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello there. I'm trying out the LIS2DS12 accelerometer. The datasheet mentions that the sensor is supposed to be able to detect a tilt, however I didn't manager to get an interrupt for such event. The datasheet doesn't give an explanation on how to u...
Hello everyone, I hope you are well and in good health.I am currently working on an academic project "Parking Barrier Command". For this application, I am going to use the MEMS sensor LIS2DW12.Checking the sonor specifications, it shows me that it ha...
Hello @Eleon BORLINI ,l want to add functionality to interrupt 2, I want that in addition to the full fifo we have. how can i do it?
Hi,I am working with STEVAL-BCNKT01V1 (Bluecoin board) with the sample project FP-SNS-ALLMEMS1 and BlueMS for android (with default configuration.) I found that there are many spikes in the mic signal occurring every 20-70ms. To make sure the hardwar...
I got a gyroscope problem when i use asm330lhh to develop a new product, and need your help.Gyroscope of ASM330LHH got abnormal output value, detail as follow.1) gyroscope zero offset is much bigger than usual.2) gyroscope noise is much bigger than u...
Dear support I need the reliability data (FIT or MTBF) for LSM6DS33 and for LPS25HB
Hello,I'm integrating the LSM6DSO32 into an MCU project and I'm using the example drivers from CubeMx.The problem is that I don't understand how the gyroscope sensitivity is calulated into the drivers. The constants for the sensitivities at the vario...
Hi,I have made a module using ISM330DLC IC. I made the schematic by taking reference from STEVAL-IDP005V1 schematic. PFA, both the schematics.Now, I am using Nucleo -F44RE board to interface this module using SPI.Also, using the libraries for the ISM...
Hi I am training to carry out a project using the MEMS library (Application DynamicInclinometer) with kit IKS01A3 and STM32WL55JC1, I have made all the configuration, the problem is that when I compile the code with STM32CUBEID, it displays this err...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.