MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Always High vibration in Z axis IIS3DWB accelerometer

I have got 2 new IIS3Dwb IC from same lot , I made custom PCB for those, connected to shaker and getting acceleration values and showing it through my own developed application.Problem: Z axis seems defecting /sensitive much higher than x and y axis ...

0693W00000Bd1XXQAZ.jpg 0693W00000Bd1TVQAZ.jpg 0693W00000Bd1UiQAJ.jpg 0693W00000Bd1TuQAJ.jpg
SMaju.1 by Associate II
  • 12659 Views
  • 24 replies
  • 1 kudos

trying to interface with an HX711 load cell amp

The HX711 requires the MCU to send an exact number of clock pulses to capture a 24 bit value, then the clock signal must remain low until the HX711 indicates its ready to transmit again, using the data line. I tried to use a GPIO pin to generate the ...

GrantW by Associate II
  • 18819 Views
  • 28 replies
  • 0 kudos

POSITION ESTIMATION

I am working with DatalogFusion application and I can see the parameters quaternion, rotation,gravity,linear_acceleration,...Assuming the errors of this kind of measurements, Wich is the best option to estimate the 2D position for a vehicle, using t...

RBAGU.1 by Associate II
  • 1217 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-STWINKT1 ML ON Microprocessor not ISM330DHCLX

I have a STEVAL-STWINKT1 board and I want to create a ML algorithm for the board to conduct predictive maintenance. However, I want my ML algorithm to run on the microprocessor and not on the ISM330DHCLX sensor. This is because, I realized that the I...

NRaha.1 by Associate II
  • 1509 Views
  • 1 replies
  • 0 kudos

Resolved! Does lsm6dsox provide some pin similar as NRST for hardware reset?

Besides the SW_Reset in CTRL_3 register, can we also do the hardware reset for lsm6dsox through some pins? Or the power gate is only option we can use?The chip worked perfectly on our device, however, in some rare cases, the registers, including whoa...

YYuan.1 by Associate II
  • 1616 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.